Configure hyperlinks
FactoryTalk
e
Procedure® instructions allow for the
configuration of hyperlink descriptors and defaults to associate them with resource
types.To configure hyperlinks
- Open FactoryTalk Administration Console and sign in to the FactoryTalk Network Directory.
- InFactoryTalk Administration Console Explorer:
- To configure a new FactoryTalk Batch Server, right-click the application or the area name and select .
- To edit an existing FactoryTalk Batch Server, expand an application or area name, right-click, and selectProperties.
- From theFactoryTalk Batch Services Propertiesdialog,Descriptors and Defaultstab, see theHyperlinks descriptors and defaultsarea.
- Select the desired resource type.
- In theDescriptorsarea, type a descriptive name for each hyperlink you want associated with the resource type.
- If necessary, type or change the information listed in theDefault Valuesfields.
- SelectOK.
- Open the FactoryTalk Batch Equipment Editor.
- Navigate to the desired resource and right-click to display the edit dialog.
- Select theHyperlinkstab.
- In theHyperlink Configurationarea, type each hyperlink. An example is,http://ServerName/eProcedure/Reports/<doc_name>where<doc_name>is the desired HTML file to display,Server_Nameis the name of the computer andReportsis a directory underProgram Files (x86)\RockwellSoftware\Batch View Server\customercontent.
- SelectOKwhen done.
- Restart the FactoryTalk Batch Server andeProcedure Server services to apply the configuration updates. When the resource is used in a batch and viewed in FactoryTalk Batch View, the hyperlink is displayed to the right of the resource.TIP: If there are batches on the batch list, theFactoryTalk BatchServer should be restarted in either Warm Restart, Warm All Restart, or Hot Restart mode. Before you restart the eProcedure server, uncheck the Cold Restart checkbox.
- Stop and restart the FactoryTalk Batch View Server.
- When you select the hyperlink, the specified web page opens. To return to FactoryTalk Batch View, selectBackon the browser toolbar. The URL displays in the remote Client’sAddressbox.
Provide Feedback