Edit the user.asp

The
User.asp
file is located in the
\Program Files\Rockwell Software\Batch\web
directory on the
FactoryTalk Batch
Server computer. You can modify this file to support requirements specific to your system. For example, you could add HTML code to the
User.asp
that links
e
Procedure
to displays of other manufacturing applications, such as status information from a SCADA (supervisory control and data acquisition) system. The
User.asp
can be modified so that documents are always available (because they are not related to specific equipment). You can also modify the
User.asp
to specify a timeout period for the Batch List ActiveX control. (For more information on specifying the timeout period, see Specifying the timeout period later in this chapter.)
IMPORTANT: Do
not
edit any ASPs other than
User.asp
. They are directly related to the successful operation of
e
Procedure
.
Other documents could be maintenance schedules, quality lab schedules, personnel shift schedules, pages for e-mail sent to the area, or web mail e-mail sender pages (to allow the operator to send e-mail from the area). You could even point them to stock pages, where the company’s stock price and press releases are posted. You could also add HTML that displays buttons linking to other manufacturing applications like an HMI or LIMS (laboratory information management systems).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal