FactoryTalk Event Archiver

The
FactoryTalk
Event Archiver's purpose is to translate the
FactoryTalk Batch
tab-delimited ASCII electronic batch record files to a user-specified file type. These electronic batch record files are maintained separately for each batch created and viewed with a word processor or spreadsheet. Many plants have standardized on one of the many commercially available Relational Database Management System (RDBMS) software packages. We recommend using a high-performance database, such as
SQL Server®
, due to their better robustness and performance. The Archiver collects data from each electronic batch record file and stores it in the specified RDBMS database format.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal