FactoryTalk Batch Equipment Editor
The
FactoryTalk Batch Equipment Editor
is a graphical interface through which a database of process equipment is defined and
maintained (an area model). - Components defined in theFactoryTalk Batch Equipment Editorare used to interface with process-connected devices (PCDs) in the facility. During recipe configuration, the area model provides a list of available units and phase classes.
- Configure phases and commands to trigger an electronic signature request when a report or recipe parameter is out of range (parameter deviation), or when specific commands are executed on a batch (such as Abort Batch or Active Step Change).
- During recipe verification, the area model confirms that the designated equipment is capable of executing the procedures.
- During recipe execution, resource arbitration functions use the area model to allocate equipment based on recipe and operator requests.
- The area model is available to all otherFactoryTalk Batchapplications.
In addition to the area model, the
FactoryTalk Batch Equipment Editor
allows configuration of the following:- Communication functions
- Electronic signatures
- Enumeration sets
- Data servers
- Recipe approvals
- Recipe version control
- FactoryTalk Event Archiverfunctions
Provide Feedback