FactoryTalk Batch Recipe Editor
The
FactoryTalk Batch Recipe Editor
is used to graphically create and configure recipes. - The interface is based on IEC 61131-3 sequential function charts (SFC) that graphically organizes recipes into procedures, unit procedures, operations and phases along with any applicable comments.
- In addition to the SFC view, theFactoryTalk Batch Recipe Editoroffers a table view. Table-based recipes provide a mechanism for creating simple recipes that do not require a complex recipe structure or elaborate transition expressions. Additionally, you can view table-based recipes and edit all recipe parameters without having to navigate between steps.
- TheFactoryTalk Batch Recipe Editorallows you to specify sequences of phases. The actual phase logic must be configured in the process-connected device (PCD) while the interface to the PCD must be configured in theFactoryTalk Batch Equipment Editor.
- Recipe reports can be generated in SFC and/or descriptive format.
- If Recipe Approvals are enabled in the underlying area model, approval signoffs are executed in theFactoryTalk Batch Recipe Editor.
- When Recipe Version Control is enabled, a version of a recipe (a read-only, numbered snapshot of a recipe) can be saved and protected from further editing. New work-in-progress (WIP) copies of a version allow the recipe author to continue to make changes and updates to a recipe. When a versioned recipe no longer matches the underlying area model, or references a deleted or non-existent sub-recipe, it is marked as obsolete.
Provide Feedback