FactoryTalk Batch Server
The
FactoryTalk Batch
Server is the engine that runs FactoryTalk Batch
. It is the component that controls system information, phases and recipes. The server
allows integration with process-connected devices (PCDs) and third-party software packages.
Prior to opening FactoryTalk®
Batch View™
, the FactoryTalk Batch
Server must be running and remain active during all batch functions.The
FactoryTalk Batch
Server operates as a Windows®
service, which means that the FactoryTalk Batch
Server can be configured to start automatically and that control of the FactoryTalk Batch
Server can be given to the Windows®
Service Manager. Because the
FactoryTalk Batch
Server runs as a service, it does not require an operator to log on to run. Therefore,
logging on or off Windows during operation does not disrupt the performance of the FactoryTalk Batch
Server.Provide Feedback