FactoryTalk Batch Network Editor
The
FactoryTalk® Batch
Network Editor is installed on the FactoryTalk Batch
Material Server computer. It is used with the FactoryTalk Batch
Material Manager to indicate the location of the Material
database.
TIP:
Starting in
FactoryTalk Batch
version 18.00.00,
the FactoryTalk Batch
Network Editor is no longer used to configure the locations of
FactoryTalk Batch
Servers. Configure FactoryTalk Batch
Server locations in
the FactoryTalk® Directory
. The Network Editor is only used with Material Manager
in version 18 and later.Provide Feedback