Benefits of eProcedure
e
ProcedureFactoryTalk
e
ProcedureThe following describes a typical recipe execution process, with and without :
e
ProcedureWithout e Procedure | With e Procedure |
|---|---|
A master recipe (a collection of SOPs) is maintained in written form. The master
recipe includes instructions for the operator, places to enter data, and places
for any required signatures. | A master recipe is created and maintained electronically with the FactoryTalk Batch Recipe Editor. The master recipe includes operator instructions, report data,
and prompts for required approvals. |
When a batch needs to be run, the recipe is printed and given to the operator,
who reads the instructions, manually sequences the process and enters the required
information on the printout. | When a batch needs to be run, the operator adds a batch using FactoryTalk Batch View , steps through the instructions, and enters the required data into the
system. |
When the batch is complete, the completed recipe document is filed. | When the batch is complete, the electronic batch record contains a complete
record of the entire batch process. |
The data can be manually entered into a database for recording and reporting
purposes. | The electronic batch record can be automatically transferred to any
ODBC-compliant database using the FactoryTalk Event Archiver. |
FactoryTalk
e
Proceduree
ProcedureThe
FactoryTalk Batch
Equipment Editor is used to define the process equipment, both manual and automated. The
modular approach in defining equipment is as appropriate with manual facilities as it is in
automated facilities. As part of the configuration process, attach instruction files to each
of the manual equipment modules.Instruction files are HTML files that include all of the required control steps for a phase. Each control step can include textual instructions, embedded parameter values, report fields for operator input, and submit buttons. Control steps may also include any valid HTML component.
Once the equipment is defined, and the instruction files are created, create recipes in the same fashion as a completely automated facility.
FactoryTalk
e
Procedure Microsoft®
Internet Explorer®
. With e
ProcedureProvide Feedback