Update the area model
You must add a new data server definition to your area model, as well as add the new phase and associated equipment module.
To update the area model:
- Open the area model in which the new phase will be used.
- From theEditmenu, selectDataServer, or select theEdit Data Serverstoolbar.
- On theDataServersdialog box, selectAdd.
- On theAdd Data Serverdialog box, enter the new data server definition name in theNamebox.
- From theTypelist, selectPC Phase OPC.The default values for the data server type are displayed. TheWatchdog Item Namemust beWATCHDOG. Any string may be used for theWatchdog Item Access Path, but the same string must be used in the PC-based phase’sTopicproperty.
- Enter the following information for the new data server definition and then clickOKto return to theDataServersdialog box:
- Watchdog Item Access Path:Phase(user-definable)
- Watchdog Item Name:watchdog
- Create a phase to be used as the PC-based phase. Assign the required number of parameter, report, and request tags. Generally, these would be equal to the number assigned to the PC-based phase’s properties.
- Create an instance of this phase in the appropriate units. Be sure to use the same name for the equipment module as theNameproperty defined for the PC-based phase.
- Assign the new data server definition to each of the tags in the newly defined equipment module. Do not change theItemnames. These should follow standard conventions and start with the name assigned to the instance of the control in the container application.
- Save the area model with the new changes.
Provide Feedback