Run a recipe with a PC-based phase
The PC-based phase executable must be active when the recipe is processed.
To run a recipe with a PC-based phase:
- Start the PC-based phase executable.
- Start theFactoryTalk BatchServer.
- Open theFactoryTalk BatchView or HMI application.
- Create a batch from the recipe containing the PC-based phase.
- Run the batch. The recipe phase interacts with the PC-based phase and performs its pre-programmed functions.The icon that represents the phase changes color based on the state of the phase. These color changes match the colors used in theFactoryTalk BatchView.
Provide Feedback