Properties
The following tables provide a summary of the properties associated with the
Batch Phase Execution
control and a description of each property.Property summary
Property | Indexed | Type | Read-only | Can be changed at design time? | Can be changed at runtime? | Tag |
|---|---|---|---|---|---|---|
CheckPointEnable | No | Boolean | No | Yes | Yes | None |
ClearRequest | No | Boolean | No | Yes | Yes | None |
Command | No | Long | — | No | No | Phasename_OC |
DDEBaseTagName | No | String | No | Yes | Only before initialization | None |
DownloadRequest | No | Boolean | Yes | No | No | None |
ExternalCommand | No | Long | No | No | Phasename_EC | |
Failure | No | Long | No | No | Phasename_F | |
Interval | No | Long | No | Yes | Only before initialization | None |
LogFileName | No | Text | No | Yes | Yes | None |
Name | No | Text | No | Yes | No | None |
NumberOfParameters | No | Long | No | Yes | Only before initialization | None |
NumberOfReports | No | Long | No | Yes | Only before initialization | None |
NumberOfReqData | No | Long | No | Yes | Only before initialization | None |
Owner | No | Boolean | No | No | Only after initialization | Phasename_W |
Parameter(N) | Yes | Text | No | No | Only after initialization | PhasenamePnn |
Pause | No | Boolean | Yes | No | No | Phasename_P |
Paused | No | Boolean | No | No | Only after initialization | Phasename_PD |
Report(N) | Yes | Text | No | No | Only after initialization | PhasenameRnn |
Request | No | Long | No | No | Only after initialization | Phasename_RQ |
RequestData(N) | Yes | Text | No | No | Only after initialization | PhasenameQnn |
RestoreRequest | No | Boolean | No | Yes | Yes | None |
SingleStep | No | Boolean | Yes | No | No | Phasename_SS |
Status | No | Long | Yes | No | No | Phasename_ST |
StepIndex | No | Long | No | No | Only after initialization | Phasename_SI |
StepIndexBuffer | No | Long | No | No | Yes | None |
StepIndexInitialValue | No | Long | No | Yes | Yes | None |
Topic | No | Text | No | Yes | Only before initialization | None |
Unit | No | Long | Yes | No | No | Phasename_UN |
UseDefaultDDETag-Name | No | Boolean | No | Yes | Only before initialization | None |
WatchdogFailureValue | No | Long | No | Yes | Only before initialization | None |
WatchdogStatus | No | Boolean | Yes | No | No | None |
WatchdogTimeout | No | Long | No | Yes | Only before initialization | None |
Property description
Property | Description |
|---|---|
CheckPointEnable | User configurable flag. When set to TRUE, a checkpoint file is updated as needed with all pertinent runtime parameters. The checkpoint file is an internal reference file that is not user-modifiable. The file is updated after each scan if a property change is seen. This file is then loaded when the phase application is started, or when the CheckPoint method is called. When set to FALSE, a checkpoint file is not maintained. The default value is TRUE . |
ClearRequest | User configurable flag. When set to TRUE, any pending request by the phase logic is canceled when a change of state is initiated. This property should be used in conjunction with the RestoreRequest property. The PLI will not allow ClearRequest to be FALSE and RestoreRequest to be TRUE (the request would be issued twice in this case). The default value is TRUE . |
Command | Contains the command information as received from the FactoryTalk Batch Server. The phase responds to this command register when the phase is in program control (owned by the FactoryTalk Batch Server). This parameter is reset after each PLI scan, so its contents are NOT indicative of the last command sent by the FactoryTalk Batch Server. |
DDEBaseTagName | Used as the base for tag names when the UseDefaultDDETagName property is set = FALSE and DDEBaseTagName property is not null. For example, if this property is set = BOO, and the UseDefaultDDETagName property is FALSE, then the tag for the phase state is BOO_ST. If this property is empty, the Name property is used as the tag name base regardless of how the UseDefaultDDETagName property is set. |
DownloadRequest | Flag set by the PLI if the FactoryTalk Batch Server has sent a DOWNLOAD command to the phase. The Server sends a DOWNLOAD command when there is a Transfer of Control condition between two consecutive equipment modules (phase instances) based on the same phase. An example would be two consecutive agitation phases where a change in agitation speed is desired when a tank level has reached a certain point.The default value is FALSE . |
ExternalCommand | Contains the command information as received from an external source (an HMI, for example). The phase responds to this command register when the phase is in external control (NOT owned by the FactoryTalk Batch Server). The default value is 0 . |
Failure | The Failure property is set within the phase logic as desired when there is an error condition that should cause the phase to be HELD. When this property is set to any value greater than zero, the PLI will execute the HOLDING sequence. The PLI will also set this property to the WatchdogFailureValue when the watchdog status is bad and will HOLD the phase. The valid range is 0 to 32767.The default value is 0 . |
Interval | Determines the execution interval (in milliseconds) of the PLI and phase logic. (This value should be the number of seconds multiplied by 1000.) The default value is 1000 . |
LogFileName | File name prefix (.LOG is added by the phase execution control) for the activity log file. The default value is BATCHPHS . |
Name | Name of the equipment module. This property must match the name given to the equipment module in FactoryTalk Batch Equipment Editor . Parenthesis created for control arrays are ignored. The default value is Phase1 . |
NumberOfParameters | Indicates the number of parameter tags that will be available to the phase. Generally, this value will be equivalent to the number of parameter tags assigned within FactoryTalk Batch Equipment Editor . The valid range is 0 to 999.The default value is 5 . |
NumberOfReports | Indicates the number of report tags that will be available to the phase. Generally, this value will be equivalent to the number of report tags assigned within FactoryTalk Batch Equipment Editor . The valid range is 0 to 999. The default value is 5 . |
NumberOfRequestData | Indicates the number of request data tags that will be available to the phase. Generally, this value will be equivalent to the number of request data tags assigned within FactoryTalk Batch Equipment Editor . The valid range is 0 to10. The default value is 5 . |
Owner | Determines phase ownership. When set to TRUE, the phase is in External control and will respond to the contents of the ExternalCommand property. When set to FALSE, the phase is owned by the FactoryTalk Batch Server and will respond to the Command property. The default value is FALSE . |
Parameter(N) | Phase parameters, where the total number (N) is specified in the
NumberOfParameters property. These are downloaded from the FactoryTalk Batch Server by placing the appropriate values into
the Request property. A NULL string is returned if Initialize has not yet
been called; Invalid index is returned when an illegal (out of range) index is
used. [Refer to the for
details.] |
Pause | The Pause property (pausING) is set by the PLI when the Pause command is
received, or when single-step mode is activated. [Refer to the FactoryTalk Batch
Server API Reference Manual , publication BATCH-RM003 The default value is FALSE . |
Paused | Set within the phase logic as desired to place the phase in the Paused state. A
Resume command must be issued to continue phase execution when the Paused
(pausED) property is set. [Refer to the for details.]The default value is FALSE . |
Report(N) | Report parameters, where the total number (N) is specified in the NumberOfReports property. Report parameters are set within the phase logic to upload report values to the FactoryTalk Batch Server for archiving. The phase logic must store report values to this property and then store an Upload Request to the Request property. A NULL string is returned if Initialize has not yet been called; Invalid index is returned when an illegal (out of range) index is used. |
Request | Used to make requests to the FactoryTalk Batch Server to accomplish a wide range of tasks
such as downloading and uploading parameter and report values. Phase logic stores
a predefined request value to this property to initiate action by the Server. This
property value must be equal to zero before storing a valid request into this
property. This property will return to zero when the Server has completed the
requested action. [Refer to the
for details.] The valid range is 1000 to 2147483648.The default value is 0 . |
RequestData(N) | Request data parameters, where the total number (N) is specified in the NumberOfRequestData property. The RequestData property performs two functions:
A NULL string is returned if Initialize has not yet been called; Invalid
index is returned when an illegal (out of range) index is used. [Refer to the
for details.] |
RestoreRequest | User configurable flag. When the phase transitions from RESTARTING to RUNNING, this property (when TRUE) will cause the request that was pending at the time the phase was HELD to be restored and executed. This property should be used in conjunction with the ClearRequest property. The PLI will not allow ClearRequest to be FALSE and RestoreRequest to be TRUE (the request would be issued twice in this case). The default value is TRUE . |
SingleStep | Flag toggled by the PLI when it receives a SingleStep command. When
single-stepping is turned ON, the Pause (pausING) property is set to TRUE
if the phase has been in the free-running state. This combination is referred to
as the single-step pausing state. When single-stepping is turned OFF, both the
Pause (pausING) and Paused (pausED) properties are cleared (set to FALSE) and the
phase return to the free-running state. [Refer to the for details.]The default value is FALSE . |
Status | Contains a numerical value that represents the current phase state. The following are the possible values with the corresponding state:
The default value is 100 . |
StepIndex | Set equal to the StepIndexInitialValue property by the PLI when the phase is STARTed or RESET. The phase logic may use this property to control program flow. The default value is 1 . |
StepIndexBuffer | Used by the PLI to save the StepIndex property when the phase is HELD. The StepIndex is restored from the StepIndexBuffer when the phase is RESTARTED. The default value is 0 . |
StepIndexInitialValue | Default value of the step index. The PLI initializes the StepIndex property to the StepIndexInitialValue value when the START or RESET command is received. The default value is 1 . |
Topic | This is the Watchdog Item Access Path as defined in a OPC server within the area model. You may define multiple OPC servers to be used with PC-based phases. They do not need to use the same topic. You may also use multiple instances of a control within one project and refer to different OPC servers. If the Topic property is set at runtime, it must be set before the Initialize method is called. The default value is BATCH . |
Unit | Contains the UnitID of the unit that controls the phase. The default value is 0 . |
UseDefaultDDETagName | User configurable flag. When set to TRUE, or when the DDEBaseTagName property is not null, the content of the Name property is used as the base for tag names. When set to FALSE, and the DDEBaseTagName property is not null, then the content of the DDEBaseTagName property is used. |
WatchdogFailureValue | This is the value that the Failure register is set to when the WatchdogStatus is bad. The value used here should then be defined within the phase_failure enumeration set in the area model. This property can be set to 0, which will turn off the hold on watchdog failure logic; the phase will not be HELD when the WatchdogStatus goes bad. The valid range is 0 to 2147483648. The default value is 13 . |
WatchdogStatus | Current status of the watchdog between the FactoryTalk Batch Server and the phase. A zero (FALSE) indicates that the status is bad and communications are down. The PLI will set the Failure property to 13 when the WatchdogStatus is bad. The default value is FALSE . |
WatchdogTimeout | Interval, in seconds, between watchdog checks by the PLI. If the WatchdogTimeout property is set at runtime, it must be set before the Initialize method is called. The valid range is 5 to 1800 seconds.The default value is 20 .The timeout period is configurable in the FactoryTalk Administration
Console . From the FactoryTalk Batch Services
Properties dialog go to the General tab or
Secondary Server tab and select OPC
communications timeout . The default time period is 10 seconds. The
PCD timer should be set to a value slightly larger than the product of the
Period (msec) and the Allowable
failures . |
Provide Feedback