Add the new phase to a recipe
Use
FactoryTalk Batch Recipe Editor
to add the new phase to a recipe.To add the new phase to a recipe:
- OpenFactoryTalk Batch Recipe Editor.
- Open the recipe where you want to add the new phase.
- Add the phase and associated transition to the recipe.
- Verify and save the recipe.
Provide Feedback