Create a new project

Use Microsoft
Visual C++
to add the
Batch Phase Execution
control to a project.
To create a new project:
  1. Start the MFC AppWizard executable.
  2. Select the
    Dialog Based
    option.
  3. Ensure that support for ActiveX Controls is selected.
  4. Use MFC as a shared DLL.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal