Add a member variable derived from the Phase Control Class

Use MFC to add a member variable derived from the
Phase Control Class
.
TIP:
The category is
Control
, and the variable type is the
Phase Control Class
. Use the appropriate resource ID as assigned to the instance of the control in the dialog.
To add a member variable derived from the Phase Control Class:
  1. Using the Class Wizard, add a member variable to the project’s dialog class.
  2. Repeat for each phase (each instance of the control).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal