Set custom properties in the Property Pages dialog box

Use the
Property Pages
dialog box to set custom properties to enable communication between a PC-based phase and the
FactoryTalk Batch
Server.
IMPORTANT:
If you attempt to configure a property at design time with an invalid entry, you are notified of the error by a message box, which includes a range of valid entries.
If you attempt to configure a property at design time that does not support configuration at design time, a message box opens.
If you attempt to configure a property at runtime that does not support modification at runtime, an entry is written to the activity log file.
To set custom properties in the Property Pages dialog box:
  1. Right-click the
    Batch Phase Execution
    control and select
    Properties
    . The
    Property Pages
    dialog box opens with the
    Configuration
    tab selected.
    FTB_PCB_Property Pages_Configuration
  2. Enter the values for the custom configuration properties.
  3. Select
    Apply
    .
  4. Select the
    Operation
    tab and enter the values for the custom operation properties.
    FTB_PCB_Property Pages_Operation
  5. Select
    Apply
    , then
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal