Add the Batch Phase Execution control to a Microsoft Visual Basic project

The
Batch Phase Execution
control must be added to the
Visual Basic
toolbox in order to make it available to your project. The instructions included here define the steps for manually adding the control to the toolbox after starting a new project. However, if you choose, you may configure the control to load automatically.
To add the Batch Phase Execution control to a Visual Basic project:
  1. Start
    Visual Basic
    .
  2. From the
    Projects
    menu, select
    Components
    .
  3. On the
    Components
    dialog box, select the
    Controls
    tab. The available Custom Controls are displayed in a list.
  4. Scrolling through the list, locate and select the
    Batch Phase Execution
    control.
  5. Click
    OK
    to close the dialog box. The
    Batch Phase Execution
    control is available on the
    Visual Basic
    toolbox. It is marked with a picture of a valve.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal