Profile

Access
Profile
to:
  • View a logged-in user and its assigned groups
  • Change the default language
  • Enable or disable the minimal view
  • View authorization settings
Try it: View profile information
  1. Select
    Profile
    .
  2. To change the default language for Batch View, select a language from the list.
    TIP:
    • Viewing the profile from within the full HMI User Control, the language settings are unavailable. HMI User Controls Language settings are controlled by FactoryTalk View SE.
    • Only languages configured for the application display in the menu.
  3. In the
    DisplayType
    , select
    Minimal
    or
    Normal
    .
    Normal
    is the default display type.
    TIP: Changing the Display Type applies to Batches and Prompts only.
  4. View the list of authorizations allowed for this profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal