Supported area model changes for non-Cold Restart
This section lists properties of an area model that can be edited without affecting a
non-Cold Restart (for example, Warm Restart, Warm All Restart, or Hot Restart) of the
FactoryTalk Batch
Server.
IMPORTANT:
If an option or parameter is not listed in this section, it is not considered safe to
modify (create, edit, or delete) that object in order to ensure a successful non-Cold
Restart of the
FactoryTalk Batch
Server.Provide Feedback