FactoryTalk Batch features

PhaseManager
adds these features to the
FactoryTalk Batch
software:
  • Common Industrial Protocol (CIP) support
    The
    FactoryTalk Batch
    Server can sequence equipment phases in
    Logix 5000
    controllers using the industry standard CIP (Common Industrial Protocol). In
    FactoryTalk Batch Equipment Editor
    , add a
    Logix5000
    CIP data server for each
    Logix 5000
    controller that contains
    PhaseManager
    equipment phases.
  • Equipment phase synchronization
    Synchronize the area model in
    FactoryTalk Batch Equipment Editor
    with the project file in
    Logix Designer
    . Create or update an equipment phase once in either application and add or update it to the other application by synchronizing the
    FactoryTalk Batch
    area model with its corresponding
    Logix Designer
    project file.
  • Navigation from FactoryTalk Batch Equipment Editor to phase logic in a Logix Designer project
    Directly navigate from a phase in
    FactoryTalk Batch Equipment Editor
    to corresponding phase logic in the
    Logix Designer
    project file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal