Open phase logic in Logix Designer

PhaseManager
gives the ability to double-click a phase in
FactoryTalk Batch Equipment Editor
and directly view and edit its phase logic in
Logix Designer
.
Logix Designer
opens to the equipment phase in the project file that corresponds to the phase selected in
FactoryTalk Batch Equipment Editor
. It is not necessary to manually open
Logix Designer
and navigate to the equipment phase to view or edit the phase logic for a phase in
FactoryTalk Batch
.
  • If the phase has a corresponding equipment phase in
    Logix Designer
    with existing phase logic,
    Logix Designer
    opens the project file to the Running routine of the equipment phase.
  • If the phase has a corresponding equipment phase in
    Logix Designer
    , and the phase logic has not been developed yet,
    Logix Designer
    opens the project file to the equipment phase.
  • If the phase does not have a corresponding equipment phase in
    Logix Designer
    ,
    Logix Designer
    opens the project file for the CIP data server that is assigned to the phase.
    TIP:
    To open the
    Logix Designer
    project file from
    FactoryTalk Batch Equipment Editor
    , the correct revision of
    Logix Designer
    must be installed on the same computer as
    FactoryTalk Batch Equipment Editor
    with an activation for each product.
    The
    PhaseManager
    activation is included in the
    Logix Designer
    Professional Version, but other versions of
    Logix Designer
    require a separate
    PhaseManager
    activation to enable the
    PhaseManager
    features in
    Logix Designer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal