Eliminates duplicate configurations

In a
FactoryTalk Batch
system using the OPC communication protocol and the
Logix Designer
programming software, manually enter communication tag data for each of the ten standard tags and for each parameter, report, and additional request tag on each phase in
FactoryTalk Batch Equipment Editor
. In
Logix Designer
, manually create the corresponding tags. Each
Tag Name
entered in
Logix Designer
must match the
Tag Item Name
entered in
FactoryTalk Batch Equipment Editor
. Additionally, in
Logix Designer
manually create the tags required for the PLI and
FactoryTalk Batch
Server communications.
In a
FactoryTalk Batch
system using
Logix Designer
with
PhaseManager
, the
FactoryTalk Batch
Server communicates directly to the equipment phase objects in the
Logix5000
controller; therefore, it is not necessary to enter any communication tag data in either application. In
FactoryTalk Batch Equipment Editor
, tag names that match the parameters and reports defined on the phase are automatically created for each phase.
PhaseManager
creates phases in
FactoryTalk Batch Equipment Editor
or equipment phases in
Logix Designer
, and synchronizes the
FactoryTalk Batch
area model with the
Logix Designer
project file. When synchronizing the area model with the project file, data types and tags are automatically created for each equipment phase and for all parameters and reports in
Logix Designer
. It is not necessary to enter this information twice, in
FactoryTalk Batch
and in
Logix Designer
, as is required if OPC data servers are used with
FactoryTalk Batch
.
Any new equipment phases added in
Logix Designer
, or modifications to existing equipment phases in
Logix Designer
, can also be transferred to the
FactoryTalk Batch
area model when the
FactoryTalk Batch
phases are synchronized with the
Logix Designer
project.
NOTE:
Unsigned data types introduced in
Logix5000
version 32.00 are not supported by
FactoryTalk Batch
. Configuring a
FactoryTalk Batch
tag to reference a controller tag of any unsigned data type (USINT, UINT, UDINT, ULINT) will result in bad communication. If you attempt to run batches referencing any tags that include one of these data types a communication failure occurs at the point when the tag is used.
Use
FactoryTalk Batch
Tag Verify
to produce a report that identifies any issues with the tag(s).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal