Open equipment phase in Logix Designer
Now that equipment phases in the
Logix Designer
project are created, open those equipment phases in Logix Designer
from their corresponding phases in FactoryTalk Batch Equipment Editor
.To open an equipment phase in Logix Designer from FactoryTalk
Batch Equipment Editor:
- InFactoryTalk Batch Equipment Editor, place the pointer over a phase that was just created in theLogix Designerproject. The pointer changes to theLogix Designerequipment phase symbol.
- Double-click the equipment phase symbol over the phase.Logix Designeropens to the selected equipment phase in the project.
- Next, develop phase logic for the equipment phases created in theLogix Designerproject.
Provide Feedback