Lot standard attributes

Lot standard attributes include:
Lot standard attributes
Name
Description
Data Type
Index
PLI Access
ID
Unique Primary Key for a lot
Integer
1
Read
Name
Lot name
String
2
Read
Controller ID
Integer ID for phase logic programmer to reference this lot
Integer
3
Read
Description
Lot description
String
4
Read/Write
EU
Engineering Units for measuring the material. Note that this data actually resides on the Material and not the Lot. The Material Server business rules are expected to return the correct value.
String
5
Read
Inventory Key
Optionally used for storing an identifier for this lot; used by third-party inventory control systems
String
6
Read
Last Edited By
The user ID (Windows logon) of the last user who changed this material data
String
7
Read
Creation Date
Time this lot was entered into the database
String
8
Read
Depletion Date
The time when this lot was completely consumed
String
9
Read
Material
Material ID value
Integer
10
Read
State
The state of the lot 1 - Lot Available for Use
Integer
11
Read/Write
Quantity
Amount of material in the lot
Real
12
Read
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal