Lot custom attribute

Lot custom attributes include:
Lot custom attributes
Name
Description
Data Type
Index
PLI Access
ID
Unique Primary Key for a lot attribute
String
1
Read
Name
Lot property name
String
2
Read
Controller ID
The ID for this attribute
Integer
3
Read
Description
Lot attribute description
String
4
Read/Write
EU
Engineering Units for measuring the material
String
5
Read
Data Type
The data type of the maximum and minimum values: Real = 0, Integer = 1, and String = 2
Integer
6
Read
Maximum
Maximum of the range of values acceptable for this material.
Real, Integer or String
7
Read
Minimum
Minimum of the range of values acceptable for this material
Real, Integer or String
8
Read
Value
The attribute value.
Real, Integer or String
9
Read/Write
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal