Upload on transfer of control reports
Configure the PXRQ instruction in
Logix Designer
to upload values for reports configured
for upload on transfer of control:External Request | Data Value Array Element | Value |
|---|---|---|
Upload Output Parameters Subset | DINT[0] | 2 |
Assign reports to this subset in
FactoryTalk Batch Equipment Editor
.If the phase associated with the report parameters enabled control strategies, only those report parameters belonging to
both
the enabled control strategy and the specified subset will be included in the upload.Provide Feedback