Upload all reports (output parameters)

Configure the PXRQ instruction in
Logix Designer
to upload values for all configured reports to the report array:
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Upload Output Parameters
DINT[0]
0
If control strategies are enabled, only those reports assigned to the recipe’s control strategy are uploaded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal