Release multiple resource values

Configure the PXRQ instruction in
Logix Designer
to release multiple resources:
PXRQ instruction configuration
External Request
Data Value Array Element
Value
Release Resources
DINT[0]
Equipment ID
DINT[1]
Equipment ID
DINT[2]
Equipment ID
Release up to 99 resources with this request. The
FactoryTalk Batch
Server releases the resources associated with the equipment IDs if this phase previously acquired the resources through an
Acquire Resources
request.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal