Send to linked phases and wait values
Configure the PXRQ instruction in
Logix Designer
to send a message to one or more linked phases and wait for a response:External Request | Data Value Array Element | Value |
|---|---|---|
Send Message to Linked Phase and Wait | DINT[0] | message ID |
DINT[1] | number of phases to receive message | |
DINT[2] | message value |
The data value array can contain up to 97 message values.
The receiving partners must issue a request before the data is sent. The sending partner may send the data at anytime. The sending phase waits for confirmation of the responses from the total number of receivers before continuing. The data is cached in the
FactoryTalk Batch
Server until the receiving partner(s) makes a request to receive the data.Provide Feedback