Send message to linked phase values
Configure the PXRQ instruction in
Logix Designer
to send a message to one or more linked phases:External Request | Data Value Array Element | Value |
|---|---|---|
Send Message to Linked Phase | DINT[0] | message ID |
DINT[1] | number of phases to receive message | |
DINT[2] | message value |
The data value array can contain up to 97 message values.
Provide Feedback