ResourcesListX
The
ResourcesListX
data item returns a directory (list) of all resources and their corresponding resource ID and type.
TIP:
For large resource lists, use the
ResourcesListX
data item. Using the ResourcesList
item for large area models may cause performance issues.Example Input of ResourcesListX: | |
|---|---|
object.GetItem(ResourcesListX) | |
Output of ResourcesListX : | |
<ResourcesListX> | |
<ResourceIndexData> | |
</ResourcesListX> | |
where ResourceIndexData is : | |
<Res ID = "Value" Type = "Value" /> | |
where: | |
Res ID (integer) – A unique Equipment ID for a Resource. Resource IDs can also be zero or negative. Zero is reserved for the Operator object and negative IDs are used for Recipe Procedures. | |
Type (positive integer) =
| |
A client request to retrieve the value of the
ResourcesListX
data item could return:<ResourcesListX><Res ID="-82" Type="5" /><Res ID="2" Type="1" /><Res ID="3" Type="2" /><Res ID="7" Type="3" /><Res ID="20" Type="4" /><Res ID="-83" Type="5" />
</ResourcesListX>
Provide Feedback