ConnectTimeout property
The
ConnectTimeout
property returns or sets the number of milliseconds the control waits for the FactoryTalk Batch
Server to acknowledge a connection before assuming that communication with the server cannot be established. The ConnectTimeout
property applies to the BatchRemote
object.Syntax | object.ConnectTimeout [= value] | |
|---|---|---|
The ConnectTimeout property syntax has these parts: | ||
Part | Description | |
object | Object expression that evaluates to a previously defined BatchRemote.RemoteSupport object. | |
value | Numeric expression specifying the length of time, in milliseconds, that the control waits for the FactoryTalk Batch Server to acknowledge a connection before assuming that communication with the server cannot be established. The default is 5000 . | |
Remarks | Setting this property to a value less than one causes an error. | |
This code example is
Visual Basic
6 syntax.Dimension a remote
FactoryTalk Batch
Server object:Dim svr As New BatchRemote.RemoteSupport
Set the ConnectTimeout period:
svr.ConnectTimeout = 4000
Provide Feedback