WarningMessage
The
WarningMessage
item returns the most recent warning message in the FactoryTalk Batch
Server’s log file.This table shows the input and output formats for this item.
Format | Description | |
|---|---|---|
Input Format | Request: WarningMessage | |
Output Format | The WarningMessage item returns in this format: <Time> \t <Description> \t <AdditionalData> | |
where: | ||
Field Name | Format | Description |
<Time> | ASCII - String | Time the message generated. |
<Description> | ASCII – String | General message description. |
<AdditionalData> | ASCII – String | More specific message information. May be <NullString> or a blank space character <sp>. |
This is an example of the return on this request.
A request on
object
.
GetItem(WarningMessage)
could return:2022.02.24 16:21:12:401 \t PARAMETER DATA SOURCE NOT FOUND \t $LABEL \crlf
Provide Feedback