UnitsList

The
UnitsList
item returns a list of all units and corresponding equipment IDs and unit classes.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
UnitsList
Output Format
The UnitsList item is returned in this format:
<UnitList>
is
<Unit>
\crlf |
<Unit>
\crlf
<UnitList>
<Unit>
is
<UnitID>
\t
<UnitName>
\t
<UnitClass>
where <Unit> is:
Field Name
Format
Description
<UnitID>
ASCII - Integer
Unique equipment identifier for a unit.
<UnitName>
ASCII - String
Unit name.
<UnitClass>
ASCII - String
Unit class name.
This is an example of the return on this request.
A request on
object
.
GetItem(UnitsList)
could return:
3 \tWP_MIXER1 \tMIXER_CLS \crlf
2 \tWP_MIXER2 \tMIXER_CLS \crlf
26 \tSP_MIXER1 \tMIXER_CLS \crlf
...
46 \tMP_MIXERFREEZER2 \tMBR_MIXERFREEZER \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal