UnitIDPhaseBitmaps

The
UnitIDPhaseBitmaps
item returns a filename list for the phase bitmaps within the unit specified by the unit ID. This is a companion item to the
UnitIDPhases
item. The files are returned in the same order as <BitMapIndex> in
UnitIDPhases
.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
UnitIDPhaseBitmaps
<UnitID>
is
ASCII – String, the unique equipment ID corresponding to the unit.
Output Format
The UnitIDPhaseBitmaps item returns in this format:
<List>
<List>
is
<BitMap>
\crlf
<List>
<BitMap>
is
<BitMapIndex>
\t
<FileName>
where:
Field Name
Format
Description
<BitMapIndex>
ASCII - Integer
Location of bit map in the List of Phase Bitmap items – same offset as returned in
UnitIDPhases
.
<FileName>
ASCII - String
Filename of the bitmap.
This is an example of the return on this request.
A request on
object
.
GetItem(55PhaseBitmaps)
could return:
0 \t dump2&.bmp \crlf
1 \t dump2&.bmp \crlf
...
5 \t t-in.bmp \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal