UnitIDOperations

The
UnitIDOperations
item returns a list of the equipment operation sequences within the unit specified by the unit ID.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
UnitIDOperations
UnitID
is
An ASCII - integer representing the
unique equipment ID corresponding to the unit.
Output Format
The UnitIDOperations item returns in this format:
<OperationsList>
is
<Operation>
\crlf |
<Operation>
\crlf
<OperationList>
<Operation>
is
<OpSeqID>
\t
<OpSeqName>
\t
<MaxOwners>
\t
<OperationType>
\t
<XCord>
\t
<YCord>
\t
<BitMapIndex>
where <Operation> is:
Field Name
Format
Description
<OpSeqID>
ASCII - Integer
Equipment ID of the equipment operation sequence.
<OpSeqName>
ASCII - String
Name of the equipment operation sequence configured in FactoryTalk Batch Equipment Editor.
<MaxOwners>
ASCII - Integer
Maximum number of owners.
<OperationType>
ASCII - Integer
This is an equipment operation sequence, so this field is not used.
<XCord>
ASCII - Integer
X coordinate for the bitmap in the Equipment View.
<YCord>
ASCII - Integer
Y coordinate for the bitmap in the Equipment View.
<BitMapIndex>
ASCII - Integer
Location of bitmap in the List of Phase Bitmap items. This field is not used.
This is an example of the return on this request.
A request on
object
.
GetItem(55Operations)
could return:
68 \t MAKE_CHOCOLATE_CUSTARD \t 1 \t 0 \t 95 \t 88 \t 0 \crlf
70 \t MAKE_VANILLA_CUSTARD \t 2 \t 0 \t 362 \t 89 \t 0 \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal