UEEventID_x
The
UEEventID_x
item returns the unique identifier assigned by the
FactoryTalk Batch
Server to the x
th unacknowledged
prompt in the unacknowledged prompts list.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: UEEventID_ <RowNumber> | ||
<RowNumber> | is | ASCII - Integer An array index. When an unacknowledged prompt generates, it adds to an array. If the
unacknowledged prompts list is not sorted, then x is the row
number of the unacknowledged prompt appearing in the unacknowledged prompts list. | |
The UEEventID_x item requires this setting in the tab: MaxPromptTableLength = n where n is the maximum number of unacknowledged prompts accessible to this item (the maximum number of entries in the array). And, where 0 £ x £ MaxPromptTableLength . If the number of unacknowledged prompts in the unacknowledged prompts list is larger than n , then this item will only access the first n unacknowledged prompts in a non-sorted unacknowledged prompts list. When an unacknowledged prompt with an index of less than n is removed from the unacknowledged prompts list, all subsequent unacknowledged prompts will have their index decreased by one. The default value of MaxPromptTableLength is 0 (zero). | |||
Output Format | The UEEventID_x item returns in this format: <EventID> | ||
where: | |||
Field Name | Format | Description | |
<EventID> | ASCII - Integer | The unique event identifier assigned by the FactoryTalk Batch Server to keep track of issued prompts. | |
This table is an example of an unacknowledged prompts list containing two unacknowledged prompts. The
Event ID
is batch data that is not displayed in the Batch List
window.Time | Batch ID | Desc | Value | Unit | Phase | Event ID |
|---|---|---|---|---|---|---|
2/24/2022 2:33:45 PM | BATCH_99 | Charge_ Amount | 35 | UA_1 | P1 | 20 |
2/24/2022 2:34:06 PM | BATCH_100 | Hold_Time | 5 | UA_2 | P44 | 21 |
This is an example of the return on this request.
For the prompt's event ID in the second row of the unacknowledged prompts list, advise on
object
.
GetItem(UEEventID_2)
could return:21
Provide Feedback