SignatureIDSig
The SignatureIDSig item returns the signature information for a single signature (excluding those generated by private interfaces).
This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: SignatureIDSig | ||
SignatureID | is | ASCII – String, the unique Signature ID corresponding to a specific signature. | |
Output Format | The SignatureIDSig item returns in this format: | ||
<SigData> | is | <ActionID> /t <CreateID> /t <SigState> /t <SigCreateTime> /t <SigEndTime> /t <SigCancelable> /t <ReqSignOffs> /t <SigType> /t <reserved1> /t <reserved2> /t <SigContext> /crlf <LastSignOff> /t <SignOffList> | |
<SignOffList> | is | <SignOff> | <SignOff> /crlf <SignOffList> | |
<SignOff> | is | <SignoffState> /t <CommentControl> /t <Meaning> /t <CompletionTime> /t <SignerName> /t <SignerID> /t <SignerComment> /t <PermissionList> | |
<PermissionList> | is | <Permission> | <Permission> /t <PermissionList> | |
<SigContext> | is | <CommandContext> | <GeneralUsageContext> | <ParamDeviationContext> | <ParamValueAckContext> | <ReportDeviationContext> | <UnitBindContext> | <UnitBindAckContext> | <PhaseBindContext> | <PhaseBindAckContext> | <RemoveContext> | <ASCContext> | <AddEventContext> | <SetParmContext> | <SetAllLabelContext> | <SetAllLotContext> | <ForceTransitionContext> | <OverrideContext> | <OverrideClearContext> | |
<CommandContext> | is | <ProcedureID> /t <Command> | |
<GeneralUsageContext> | is | <ProcedureID> /t <StepIndex> | |
<ParamDeviationContext> | is | <ProcedureID> /t <ParameterName> /t <NewValue> /t <CurrentValue> /t <DeviationType> /t <ParamLimits> | |
<ParamValueAckContext> | is | <ProcedureID> /t <ParameterName> /t <NewValue> /t <DefaultValue> | |
<ReportDeviationContext> | is | <ProcedureID> /t <ReportName> /t <UploadedValue> /t <TargetParamName> /t <TargetParamValue> /t <DeviationType> /t <ReportLimits> | |
<UnitBindContext> | is | <UnitID> /t <ProcedureList> | |
<UnitBindAckContext> | is | <UnitID> /t <ProcedureList> | |
<PhaseBindContext> | is | <ProcedureID> /t <EquipmentPhaseID> /t <ContainerName> /t <MaterialName> /t <Lot> /t <Label> | |
<PhaseBindAckContext> | is | <ProcedureID> /t <EquipmentPhaseID> /t <ContainerName> /t <MaterialName> /t <Lot> /t <Label> | |
<RemoveContext> | is | <ProcedureID> | |
<ASCContext> | is | <ProcedureID> /crlf <ActivateStepList> /crlf <DeactivateStepList> | |
<AddEventContext> | is | <ProcedureID> /t <Type> /t <Description> /t <Value> | |
<SetParmContext> | is | <ProcedureID> /t <ParameterName> /t <NewValue> /t <CurrentValue> | |
<SetAllLabelContext> | is | <ProcedureID> /t <NewValue> | |
<SetAllLotContext> | is | <ProcedureID> /t <NewValue> | |
<OverrideContext> | is | <ProcedureID> /t <Parameter Name> /t <New Value> /t <Current Value> | |
<OverrideClearContext> | is | <ProcedureID> /t <Parameter Name> /t <New Value> /t <Current Value> | |
<ForceTransitionContext> | is | <TransitionID> /t <Transition Condition Expression> | |
<ParamLimits> | is | <LLimit> /t <HLimit> /t <LLLimit> /t <HHLimit> /t <LLLLimit> /t <HHHLimit> | |
<ReportLimits> | is | <LLimit> /t <HLimit> /t <LLLimit> /t <HHLimit> /t <LLLLimit> /t <HHHLimit> | |
<ProcedureList> | is | <ProcedureID> | <ProcedureID> /t <ProcedureList> | |
<ActivateStepList> | is | <NullList> | <StepList> | |
<DeactivateStepList> | is | <NullList> | <StepList> | |
<StepList> | is | <StepName> | <StepName> | |