ResourcesList
The
ResourcesList
item returns a list of all resources and their corresponding equipment IDs.
TIP:
For large resource lists, use the
ResourcesListX
data item. Using the ResourcesList
item for large area models may cause performance issues.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: ResourcesList | ||
Output Format | The ResourcesList item returns in this format: | ||
<ResourcesList> | is | <Resource> | <Resource> <ResourcesList> | |
<Resource> | is | <ResourceID> \t <ResourceName> \t <ResourceType> \t <ArbMask> \crlf | |
where <Resource> is: | |||
Field Name | Format | Description | |
<ResourceID> | ASCII - Integer | Unique equipment ID for a resource. | |
<ResourceName> | ASCII - String | Name of the resource. (Process Cells, Units and Shared Resources are included in this list.) | |
<ResourceType> | ASCII - Integer | Type of the resource:
| |
<ArbMask> | Encoded String | Arbitration masks | |
This is an example of the return on this request.
A request on
object.GetItem(ResourcesList)
could return:-1138 \t 17:MCLS_FRENCHVANILLA\MCLS_TRANSFER_OUT_UP:1\MCLS_TRANSFER_OUT_OP:1 \t 5 \t
0 \crlf
-1137 \t 17:MCLS_FRENCHVANILLA\MCLS_TRANSFER_OUT_UP:1 \t 5 \t 0 \crlf
-1136 \t 17:MCLS_FRENCHVANILLA\MCLS_TRANSFER_IN_UP:1\MCLS_TRANSFER_IN_OP:1 \t 5 \t 0
\crlf
...
119 \t FV101 \t 4 \t 1 \crlf
Provide Feedback