ResourceIDRequesters
The
ResourceIDRequesters
item returns a list of all resource requesters and their corresponding owner IDs.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: ResourceIDRequesters | ||
ResourceID | is | ASCII - String, the | |
Output Format | The ResourceIDRequesters item returns in this format: | ||
<ResourceIDRequesters> | is | <NullList> \crlf | <RequestingList> | |
<RequestingList> | is | <Resource> | <Resource> <RequestingList> | |
<Resource> | is | <ResourceID> \t <ResourceName> \crlf | |
where: | |||
Field Name | Format | Description | |
<ResourceID> | ASCII - Integer | Unique equipment ID configured in FactoryTalk Batch Equipment Editor . If the owner is the batch operator, the ID is 0 (zero). | |
<ResourceName> | ASCII - String | Name of the Process Cell, Unit, Phase or Resource. | |
This is an example of the return on this request.
A request on
object
.
GetItem(119Requesters)
could return:0 \t OPERATOR \crlf
Provide Feedback