ResourceIDInfo

The
ResourceIDInfo
item returns the resource name denoted by the resource ID.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
ResourceIDInfo
ResourceID
is
ASCII - String, the
unique equipment ID corresponding to a specific resource. A resource is an equipment entity (Process Cell, Unit, Phase or Shared Resource).
Output Format
The ResourceIDInfo item returns in this format:
<ResourceInfo>
is
<ResourceInfo>
where:
Field Name
Format
Description
<ResourceInfo>
ASCII - String
The name of the resource prefaced with the type of resource:
Procedure (for Operator)
Process Cell
Unit
Phase
Resource
This is an example of the return on this request.
A request on
object
.
GetItem(68Info)
could return:
Phase NP_ADDDAIRY_M1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal