ProcedureIDUnitRequirements

The
ProcedureIDUnitRequirements
item returns the set of unit requirements configured within the specified recipe structure.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
ProcedureIDUnitRequirements
<ProcedureID>
is
ASCII - String, the unique path to the recipe step. This path begins with the
CreateID
. Use
BLCreateID_x
item to retrieve the
CreateID
.
for an Operation Recipe:
<Operation Level>
is
<CreateID>
for a Unit Procedure Recipe:
<Unit Procedure Level>
is
<CreateID>
<Operation Level>
is
<CreateID>
\t
Operation Name
for a Procedure Recipe:
<Procedure Level>
is
<CreateID>
<Unit Procedure Level>
is
<CreateID>
\t
UnitProcedure Name
<Operation Level>
is
<CreateID>
\t
UnitProcedure Name \t Operation Name
Output Format
The ProcedureIDUnitRequirements item returns in this format:
<UnitRequirements>
is
<NullList>
|
<UnitReqList>
<UnitReqList>
is
<UnitRequirement>
|
<UnitRequirement>
\crlf
<UnitReqList>
<UnitRequirement>
is
<UnitReqName>
/t
<UnitReqID>
/t
<UnitReqType>
/t
<UnitReqClassOrInstanceName> <AssocStepList>
/t $END
<DownstreamUnitReqList>
<AssocStepList>
is
<NullList>
| /t
<AssocSteps>
<AssocSteps>
is
<ElemID>
|
<ElemID>
/t
<AssocSteps>
<DownstreamUnitReqList>
is
<NullList>
| /t
<DownstreamUnitReqs>
<DownstreamUnitReqs>
is
<DownstreamUnitReqID>
|
<DownstreamUnitReqID>
/t
<DownstreamUnitReqs>
where <PhaseDesc> is:
Field Name
Format
Description
<UnitReqName>
ASCII - String
Unit Requirement Name
<UnitReqID>
ASCII - Integer
Unique ID assigned to Unit Requirement
<UnitReqType>
ASCII - Integer
Unit Requirement Type Code:
1 = Unit Class
2 = Unit Instance
<UnitReqClassOr
InstanceName>
ASCII - String
Name of Unit Class or Unit Instance associated with Unit Requirement
<ElemID>
ASCII - Integer
Unique ID of step associated with this Unit Requirement
<DownstreamUnit
ReqID>
ASCII - Integer
Unique ID of configure downstream Unit Requirement
This is an example of the return on this request.
A request on
object
.
GetItem(17UnitRequirements)
could return:
MAX_SPEED \t 13 \t 1 \t MIXER \t 127 \t $END \t 14 \crlf
TEMP \t 14 \t 1 \t FREEZER \t 128 \t $END
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal