PhasesList

The
PhasesList
item returns a list of all phases, corresponding equipment IDs, and valid units.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
PhasesList
Output Format
The PhasesList item returns in this format:
<PhasesList>
is
<PhaseData>
\crlf |
<PhaseData>
\crlf
<PhasesList>
<PhaseData>
is
<PhaseDesc>
\t
<UnitList>
<PhaseDesc>
is
<PhaseID>
\t
<PhaseName>
<UnitList>
is
<UnitName>
|
<UnitName>
\t
<UnitList>
where <PhaseDesc> is:
Field Name
Format
Description
<PhaseID>
ASCII - Integer
Unique equipment ID for a phase.
<PhaseName>
ASCII - String
Name of a phase.
where <UnitList> is:
Field Name
Format
Description
<UnitName>
ASCII - String
Name of the unit.
This is an example of the return on this request.
A request on
object.GetItem(PhasesList)
could return:
5 \t WP_ADD_CREAM_M1 \t WP_MIXER1 \crlf
6 \t WP_ADD_CREAM_M2 \t WP_MIXER2 \crlf
39 \t SP_ADD_CREAM_M1 \t SP_MIXER1 \crlf
...
04 \t MP_DUMP_MF2 \t MP_MIXERFREEZER2 \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal