PhaseIDStepIndex

The
PhaseIDStepIndex
item returns the current step attribute of the phase specified by the phase ID.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
PhaseIDStepIndex
Output Format
The PhaseIDStepIndex item returns in this format:
<StepIndex>
Field Name
Format
Description
<StepIndex>
ASCII - Integer
Value of the
Step Index
tag in the process-connected device.
This is an example of the return on this request.
A request on the
object.GetItem(12stepindex)
could return:
4
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal