PhaseIDPausing
The
PhaseIDPausing
item returns the PAUSING attribute for a phase or an equipment operation sequence.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: PhaseIDPausing | ||
PhaseID | is | Unique equipment ID corresponding to the phase or equipment operation sequence. | |
Output Format | The PhaseIDPausing item returns in this format: <PausingText> | ||
Field Name | Format | Description | |
<PausingText> | ASCII - String | Value in the Pausing tag in the process-connecteddevice (PCD).
| |
This is an example of the return on this request.
A request on
object
.
GetItem(68Pausing)
could return:Off
Provide Feedback