PhaseIDParms
The
PhaseIDParms
item returns all parameters for the phase. If the phase is inactive there is no data returned.This table shows the input and output formats for this item.
Format | Description | ||
|---|---|---|---|
Input Format | Request: PhaseIDParms | ||
PhaseID | is | ASCII - Integer, the unique Equipment ID corresponding to the phase. | |
Output Format | The PhaseIDParms item returns in this format: | ||
<PhaseIDParms> | is | <NullList> | <PhaseParmList> | |
<PhaseParmList> | is | <ParmEntry> | <ParmEntry> <PhaseParmList> | |
<ParmEntry> | is | <ParmName> \t <ParmType> \t <ParmScope> \t <Eus> \t <MaxValue> \t <MinValue> \t <Value> \t | |
where <ParmEntry> is: | |||
Field Name | Format | Description | |
<ParmName> | ASCII - String | Name of parameter. | |
<ParmType> | ASCII - Integer | 1: Real 2: Long Integer 3: String 5: Enumeration | |
<ParmScope> | ASCII - Integer | 1: Value 2: UnAcked Prompt 3: Deferred Parameter | |
<EUs> | ASCII - String | Engineering units. | |
<MaxValue> | ASCII - String | Maximum value. | |
<MinValue> | ASCII - String | Minimum value. | |
<Value> | ASCII - String | Current value. ??? represents an Unacknowledged Prompt | |
This is an example of the return on this request.
A request on
object
.
GetItem(68Parms)
could return:MATERIAL \t 5 \t 1 \t MATERIALS \t \t \t CREAM
Provide Feedback