PhaseIDInfo

The
PhaseIDInfo
item returns the name of the phase which is denoted by the phase ID.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
PhaseIDInfo
PhaseID
is
ASCII - Integer, the unique Equipment ID corresponding to the phase.
Output Format
The PhaseIDInfo item returns in this format: Phase
<PhaseInfo>
Field Name
Format
Description
<PhaseInfo>
ASCII - String
Name of the phase prefaced with the text Phase.
This is an example of the return on this request.
A request on
object.GetItem(68Info)
could return:
Phase NP_ADDDAIRY_M1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal