PhaseErrs

The
PhaseErrs
item lists all the phases that are currently in failure or have an error.
If the
FactoryTalk Batch
Server does not return any data when issued a request against this item, it is possible that the item is disabled in the same manner as the
PhaseDataList
item.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
PhaseErrs
Output Format
The PhaseErrs item returns in this format:
<PhaseErrors>
is
<NullList>
|
<PhErrList>
\crlf
<PhErrList>
is
<PhErrDesc>
\crlf |
<PhErrDesc>
\crlf
<PhErrList>
<PhErrDesc>
is
<PhaseID>
\t
<PhaseName>
\t
<UnitID>
\t
<UnitName>
\t
<PCellName>
\t
<AreaName>
\t
<Owner>
\t
<BatchID>
\t
<PhErrMsg>
\t
<State>
<PhErrMsg>
is
<FailMsg>
|
<ErrMsg>
where <PhErrDesc> is:
Field Name
Format
Description
<PhaseID>
ASCII - Integer
Equipment ID of the phase.
<PhaseName>
ASCII - String
Name of phase configured in
FactoryTalk Batch Equipment Editor
.
<UnitID>
ASCII - Integer
Current unit ID.
<UnitName>
ASCII - String
Current unit name.
<PCellName>
ASCII - String
Process cell name.
<AreaName>
ASCII - String
Area name.
<Owner>
ASCII - String
Owner name.
<BatchID>
ASCII - String
User-entered identifier for the batch.
<PhErrMsg>
ASCII - String
Message generated by the
FactoryTalk Batch
Server.
<State>
ASCII - String
Current state of the phase.
where <PhErrMsg> is:
<FailMsg>
ASCII - String
Failure message generated by the logic running in the PLC. It is configured in the
Phase_Failures
enumeration of the
Equipment Database
.
<ErrMsg>
ASCII - String
Error message generated by the
FactoryTalk Batch
Server. This message is internal to
FactoryTalk Batch
.
This is an example of the return on this request.
A request on
object.GetItem(PhaseErrs)
could return:
68 \t NP_ADDDAIRY_M1 \t 0 \t \t West_Parlor \t AREA1 \t \t \t FV101_FAILED_TO_CLOSE \t IDLE \crlf
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal