OPCClientCount

The OPCClientCount item returns the number of OPC clients connected to the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
OPCClientCount
Output Format
The OPCClientCount item returns in this format:
<OPCCount>
where:
Field Name
Format
Description
<OPCCount>
ASCII – String
Number of OPC clients connected to the
FactoryTalk Batch
Server.
This is an example of the return on this request.
A request on
object
.
GetItem(OPCClientCount)
could return:
2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal