MatSvrStatus
The
MatSvrStatus
item returns the status of the Material Server as an ordinal data item.This table shows the input and output formats for this item.
Format | Description | |
|---|---|---|
Input Format | Request: MatSvrStatus | |
Output Format | The MatSvrStatus item returns in this format: <Status> | |
where: | ||
Field Name | Format | Description |
<Status> | ASCII – Integer | 3 = Material Manager not installed.2 = Material Server communication in use. 1 = Material Server communication available but not restored. 0 = Material Server communication not available. |
This is an example of the return on this request.
A request on
object.GetItem(MatSvrStatus)
could
return:3
Provide Feedback