ListSeparator

The
ListSeparator
item returns the list separator used by the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input and output formats
Format
Description
Input Format
Request:
ListSeparator
Output Format
The ListSeparator item returns in this format:
<Separator>
Field Name
Format
Descriptio
n
<Separator>
ASCII – String
Default list separator for the language-specific operating system.
This is an example of the return on this request.
A request on
object.GetItem(ListSeparator)
could return:
,
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal